Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How much current is allowed to flow?

Latest Updated:08/01/2005

Question:

The absolute maximum rating of the base current of a small signal transistor is not defined. How much current is allowed to flow?

Answer:

Generally, the maximum rating of Ib is Ib ≤(1/10)Ic.
Check the base current based on the absolute maximum rating of the collector current.
Suitable Products