Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What are variations of 3 terminal over current restriction circuit?

Latest Updated:02/01/2007

Question:

What are variations of the 3-terminal regulator's overcurrent restriction circuit?

Answer:

The peak output current (IOpeak) indicates the operation starting point of the overcurrent restriction circuit. Refer to the variations of the peak output current.

Suitable Products
Bipolar Operational Amplifiers
3 Terminal Regulators