Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is channel separation?

Latest Updated:12/01/2011

Question:

What is channel separation?

Answer:

Channel separation indicates the extent to which the operating operational amplifier affects other operational amplifiers when there are multiple operational amplifiers (2 or 4 channels) incorporated in a package.

Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
M66596, R8A66597
UPD720150