Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How is the shunt regulator used?

Latest Updated:12/01/2004

Question:

How is the shunt regulator used?

Answer:

The shunt regulator is connected in parallel with the load, which has the result of shunting the current.
It detects fluctuation of the output current and input voltage by using an operational amplifier and holds the output voltage constant by controlling a variable resistor connected in parallel with the load.

Suitable Products
Power Management Linear
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
CMOS comparators
bipolar comparators