Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What does 200 A at PW ≤ 10 μs, duty cycle ≤ 1% in 2SK1522E data sheet means?

Latest Updated:09/02/2013

Question:

The 2SK1522E datasheet states a drain peak current of 200 A at "PW ≤ 10 μs, duty cycle ≤ 1%".
What does this mean?

Answer:

PW ≤ 10 μs, duty cycle ≤ 1% means that (a) during 1% (or less) of one cycle, (b) a pulse of pulse width 10 μs (or less) is applied. This means that for the 2SK1522E, under these conditions and at the rated channel temperature, the maximum drain current is 200 A.
Suitable Products
Power MOSFETs for General Switching