Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What does "-T" means in TO-92 and SP-8?

Latest Updated:04/01/2007

Question:

I have noticed that the order number for some through-hole type packages such as the TO-92 and SP-8 includes the symbol "-T". What does this refer to?

Answer:

The "-T" in the order number means a packing container with a radial taping.
In radial taping products, the interval between the lead tips differs from normal products (non-reel products) (see the figure below). For details such as package dimensions, please contact your nearest Renesas Electronics representative or distributor.

Suitable Products
  • Was this article helpful?