Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What are the materials and weight of the uPC1093?

Latest Updated:12/01/2011

Question:

What are the materials and weight of the uPC1093?

Answer:

The package is made of epoxy resin and the weight is approximately 0.29 g.
Suitable Products
CMOS comparators
bipolar comparators
Shunt Regulators