What is the thermal resistance of 2SK1292 (discontinued product)?
Latest Updated:09/02/2013
Question:
How much is the thermal resistance of the 2SK1292 (discontinued product)? It's not in the datasheet.
Answer:
The thermal resistance of the 2SK1292 is as follows.
- Channel to case thermal resistance = 3.57 ℃/W
- Channel to air thermal resistance = 62.5 ℃/W
Suitable Products
Power MOSFETs for General Switching |