Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the difference between general use and industrial use?

Latest Updated:09/01/2005

Question:

What is the difference between operational amplifiers/comparators for general use and those for industrial use?

Answer:

An operational amplifier/comparator for general use is recommended for use in consumer products, whereas one for industrial use is recommended for use in industrial equipment. The latter are designed for use in sets that operate in difficult environments and therefore have a wider ambient operating temperature range than the former. Moreover, with operational amplifiers/comparators for industrial use, all devices are subject to testing with all test items.

(Example) Single-power-supply dual operational amplifier

For general use (UPC358G2) : Ambient operating temperature range: -20 to +80°C

For industrial use(UPC1251G2) : Ambient operating temperature range: -40 to +85°C

(2005/09)

Suitable Products
Comparators