Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

In package sketch of 3-pin power mini mold, is it the top or bottom view?

Latest Updated:04/01/2007

Question:

I cannot tell if the package drawing of a 3-pin power mini mold (SC-62) is the top view or the bottom view.

Answer:

The bottom view is shown so that it is easy to recognize the pin shapes of the collector and source at the center.
Suitable Products