How are VDSS and VGSS of power MOSFETs defined?
Latest Updated:02/01/2008
Question:
How are VDSS and VGSS of power MOSFETs defined?
Answer:
VDSS is the maximum voltage that can be applied between the drain and source while the gate and source are short-circuited.

VGSS is the maximum voltage that can be applied between the gate and source while the drain and source are short-circuited.

For how to read the symbols, see How to read symbols of absolute maximum ratings.

VGSS is the maximum voltage that can be applied between the gate and source while the drain and source are short-circuited.

For how to read the symbols, see How to read symbols of absolute maximum ratings.
Suitable Products
Power MOSFETs |