Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the maximum value if the data sheet shows turn off time as 250 ns?

Latest Updated:09/02/2013

Question:

The 2SK1671 datasheet shows the turn-off time as 250 ns (TYP). What is the maximum value?

Answer:

We have not specified minimum and maximum values for switching characteristics such as turn-off time for the 2SK1671. We generally specify Typ values for switching characteristics. Thank you for your understanding.
Suitable Products
Power MOSFETs for General Switching
  • Was this article helpful?