Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Would it be possible if P- L- or M- rank will be shipped instead of N-rank?

Latest Updated:12/01/2010

Question:

For general-use photocouplers, there are various CRT ranks. N-rank products are all products with the MIN and MAX ratings in the electrical characteristics table. Does this mean that P-, L-, or M-rank products might be shipped instead of N-rank products?

n_rank.gif

Answer:

N-rank products will not be shipped in the mixes with P-, L-, or M-rank products.

Suitable Products
Photocouplers / Optocouplers