What are the output characteristics of the uPC803?
Latest Updated:12/01/2011
Question:
What are the output characteristics of the uPC803?
Answer:
Data of the uPC803 at hand were measured. The results are as shown on the left.
Use this data for your reference.
Test conditions: Room temperature (approx. 25°C)
Supply voltage: ±15 V
Note that this data is a product that happened to be at hand and that the results are not guarantee values.
Suitable Products