Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Meaning of Letters/Numbers in MOSFET, Thyristor & Diode Part Numbers

Last Updated: 06/24/2016

Question:

Is there a way to decipher what the numbers and letters mean for MOSFET, Diode & Thyristor part numbers?

Answer:

Yes, there is meaning behind the letters/numbers which make up the part number for MOSFET, Diode & Thyristor devices. For help with deciphering them, see the Orderable Part Number Guide here.
  • Was this article helpful?