Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

RDK RX63N Reference Guide & Downloads

Last Updated: 06/27/2016

Question:

Where can I download the latest complete software package for the RX63N RDK? Where can I find the user manual, gerber files & schematics? What are its target applications?

Answer:

Target applications for the RX63N RDK include gaming (3-axis accelerometer), communications (10/100 Ethernet 1588 compatible, CAN, I2C, SPI interfaces), audio, and motor control. All the materials related to the RX63N RDK can be found here. Look for the Documentation and Downloads tabs as appropriate for the user manual, gerber files & scheamtics. Note: You will need to log into your MyRenesas account or register for a free account to complete the download process.