Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What causes variation in the accuracy and precision of the low-speed on-chip oscillator?

Last Updated:12/26/2017

Question:

What causes variation in the accuracy and precision of the low-speed on-chip oscillator?

Answer:

General causes of variation are:

  • Manufacturing variation (chip variation).
  • Variation caused by supply voltage fluctuation.
  • Variation caused by ambient temperature.
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx