Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

If SI/O3 & SI/O4 set at transmit only, can SINi pin be used as an I/O port?

Latest Updated:09/22/2010

Question:

If SI/O3 and SI/O4 are set for transmit only, can the SINi pin be used as an I/O port?

Answer:

Yes, the SINi pin can be used as a programmable I/O port.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/29
M16C/28