Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

When DMA accesses external space do ICIS0 & ICIS1 influence bus timing ?

Latest Updated:03/18/2009

Question:

Bits ICISO & ICIS1 in the BCR register of the H8/3067 import idle cycles . When the DMA controller accesses external space do ICIS0 & ICIS1 influence bus timing ?

Answer:

The Bus Controller still operates during DMAC operation. If idle cycle insertion is designated by BCR the cycle is inserted at DMAC start up.
Suitable Products
H8/300H