Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

The Renesas Flash Programmer V2 and V3 at the same time?

Latest Updated:08/24/2016

Question:

Can I use both the Renesas Flash Programmer V2 and V3 at the same time?

Answer:

Yes, you can use them concurrently.

If you have Renesas Flash Programmer V2 (the commercial edition), you can update it to V3 free of charge.
If you purchase the Renesas Flash Programmer V3 (commercial edition), you can use both of them.

According to License Registration, refer to the following information.

How to resister License of the Renesas Flash Programmer V2 into the Renesas Flash Programmer V3.

Install the Renesas Flash Programmer V3 Upgrade latest version into the host PC installed the Renesas Flash Programmer V2 commercial edition.
Resister by importing a license file that is located in the License_File folder of the CD of the Renesas Flash Programmer V2 into "Import of License" of Help menu on the Renesas Flash Programmer V3.

However, license import function has not been supported on the RFP V3.00.00 yet.
It is supported on the RFP V3.01.00. Please register the license file.

How to resister License of Renesas Flash Programmer V3 into Renesas Flash Programmer V2.

Install the Renesas Flash Programmer V2 Upgrade latest version into the host PC installed the Renesas Flash Programmer V3 commercial edition.
Resister by importing a license file that is located in the License File folder of the CD of the Renesas Flash Programmer V3 into "Import of License" of Help menu on the Renesas Flash Programmer V2.

Suitable Products
Renesas Flash Programmer