Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How can I confirm the version of the toolchain I am using in HEW V.4, V.3?

Latest Updated:12/06/2010

Question:

How can I confirm the version of the toolchain I am using in my High-performance Embedded Workshop (High-performance Embedded Workshop V.4, V.3)?

Answer:

To confirm the version of the toolchain used in the active High-performance Embedded Workshop, refer here.
Suitable Products
High-performance Embedded Workshop
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for RX Family
C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA]
C Compiler Package for R32C Series
C Compiler Package for M32C Series [M3T-NC308WA]
C/C++ Compiler Package for H8SX, H8S, H8 Family