Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Projects tab can not be updated when [Build All] is chosen. Why?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.3]  File dependency of "Projects" tab on work space window is updated when Build] is from the [Build] menu . However, a it can not be updated when [Build All] is chosen. Why?

Answer:

When you choose [Build All], it does not update a file dependency. To update a file dependency, choose [Update All Dependencies] from the [Build] .

 

Suitable Products
High-performance Embedded Workshop