Why building operation did not stop even if I click execute Build in menu
Latest Updated:09/10/2007
Question:
[High-performance Embedded Workshop V.4, V.3] Even though I clicked an execute Build from the Build menu,the building operation did not stop. Why?
Answer:
Execute Build is canceled after executing the Build command for the current file(or executing the current phase) in High-performance Embedded Workshop.
Please choose [Build->Terminate Current Tool] If you don't recieve a reply after awhile from project builder, the current process may have crashed. A file which is output from a crashed tool is invalid.
Please re-execute the phase by deleting these output files.
Suitable Products
High-performance Embedded Workshop |