Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

RL78/G1D> Applications of program Flash ROM 128KB model

Latest Updated:12/28/2016

Question:

What applications can fit into the 128KB program flash memory?

Answer:

Applications that use Beacon or small memory profiles (FMP, PXP, etc.) can fit by using a code efficient compiler like CC-RL.
Suitable Products
RL78/G1D
Bluetooth