Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

RL78/G1D> Limit on number of mode transition of the Adaptable Function

Latest Updated:12/28/2016

Question:

Is there a limit on the number of the Adaptable Function mode transitions within a certain period?

Answer:

There is no limit on the number of transitions.
The mode automatically transitions with the RSSI value at that time (Low Power ⇔ Normal ⇔ High Performance).
The Adaptable Function is effective only when slave connection is active.
Suitable Products
RL78/G1D
Bluetooth