Is the "intstk" stack only used for the interrupt handler?
Latest Updated:12/01/2011
Question:
The size of "intstk" is specified in the configuration file.
Is this stack only used for the interrupt handler?
Is this stack only used for the interrupt handler?
Answer:
This is used for the interrupt handler and timer handler.
Suitable Products