Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(RX62T, RX610, RX62G, RX63T) What types of resonator can be connected and what can you recommend?

Latest Updated:08/10/2012

Question:

What types of resonator can be connected? And is there a recommended resonator?

Answer:

ceramic resonator or a crystal resonator can be used for the main clock oscillator. Please use a crystal resonator for the sub-clock oscillator. There are no particular resonators that we recommend.
Suitable Products
RX630
RX63N, RX631
RX210
RX220
RX110
RX111