Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Are there recommended resonator that can be connected?

Latest Updated:05/27/2013

Question:

What types of resonator can be connected?
And is there a recommended resonator?

Answer:

A crystal resonator can be used for the main clock oscillator and the sub-clock oscillator.
There are no particular resonators that we recommend.
Suitable Products
RX62N, RX621