Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can I use 0.1 μF as a multilayer ceramic capacitor instead of 22 μF?

Latest Updated:06/10/2013

Question:

In the RX610 or RX62N user's manual: hardware, a 0.1 μF multilayer ceramic capacitor is recommended between PLLVCC and PLLVSS. However, in the RX62T user's manual: hardware, 22 μF is recommended. Is there a problem with using 0.1 μF?

Answer:

Yes, for RX62T, a 22 μF multilayer ceramic capacitor is recommended between PLLVCC and PLLVSS.

For RX62T, PLLVCC is the POR reference voltage.
The capacitance of CPB is set to 22 μF in order to prevent misdetection of POR.

Suitable Products
RX62N, RX621
RX62T
RX610
RX62G