Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

In SCI, does dummy data needs to be written to the TDR?

Latest Updated:01/23/2014

Question:

For the serial communications interface (SCI), when performing serial reception using an external clock, does dummy data need to be written to the transmit data register (TDR)?

Answer:

If serial transmission operation is disabled by the transmit enable bit (SCR.TE), reception is possible even if dummy data is not written.
Suitable Products
RX630
RX63N, RX631
RX210