Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is there any way to reduce the error rate for SCI communication speed?

Latest Updated:01/23/2014

Question:

Is there any way to reduce the error rate for SCI communication speed? (other than by increasing PCLK)

Answer:

Other than increasing PCLK, methods to reduce the error rate are as follows.

Use SCI5 or SCI6 and select an on-chip TMR clock as the clock source.

Suitable Products
RX630
RX63N, RX631
RX210