Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

RX microcontroller able to read device information using a program?

Latest Updated:12/18/2013

Question:

Is it possible to read device identification information (part number, memory size, etc.) from an RX microcontroller using a program?

Answer:

It is not possible in the current RX series.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210