Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What can be used as an interrupt pin in normal operation mode?

Latest Updated:06/10/2013

Question:

For external interrupt pins, there are regular interrupt pins and interrupt pins for returning from deep software standby (henceforth, DSTB). Can a DSTB return interrupt pin (for example, IRQ0-DS) be used as an interrupt pin in normal operation mode?

Answer:

In normal operation mode, IRQ0-DS can be used as an IRQ0 interrupt pin.
Suitable Products
RX630
RX63N, RX631
RX63T
RX210