Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What if the data that I want to program is FFFFh?

Latest Updated:01/23/2014

Question:

For (2) under FCU Command Usage, Programming and Erasing the E2 DataFlash Memory in the E2 DataFlash Memory (Flash Memory for Data Storage) chapter of the User's Manual: Hardware, it states that "If the area accessed... includes addresses that do not require programming, write FFFFh as the programming data for those addresses". What if the data that I want to program is FFFFh?

Answer:

If you want to write FFFFh, specify FFFFh.

 

Suitable Products
RX210