Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

When using the E1 or E20 emulator, how should BSCANP pin be connected?

Latest Updated:01/23/2014

Question:

When using the E1 or E20 emulator, how should the BSCANP pin be connected?

Answer:

When using the E1 or E20 emulator, set the BSCANP pin to low (inactive) and the EMLE pin to high.
Suitable Products
RX630
RX63N, RX631