Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Will interrupt generates if deep software standby mode is cancelled?

Latest Updated:05/28/2013

Question:

When an interrupt is used to cancel deep software standby mode, is interrupt processing generated?

Answer:

Cancellation of deep software standby mode is carried out by a reset. The corresponding interrupt source is not activated after a reset. The cancellation source can be checked by referring to the deep standby interrupt flag registers (DPSIFR0 to 3, and DPSIFR).
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210