Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Are there any guidelines for mounting on a board? Also, is there a recommended number of board layers?

Latest Updated:05/09/2016

Question:

Are there any guidelines for mounting on a board? Also, is there a recommended number of board layers?

Answer:

The following guidelines for a mounting on a board are available.
・DDR3 Interface PCB Design Guide
・High speed interface PCB Design Guide(USB/PCIe/SATA) mounting guidelines
For details, please contact a Renesas sales office or representative.
Recommended numbers of board layers are as follows.
・RZ/G1N, RZ/G1M: 8 layer build-up
・RZ/G1E: 6 layer build-up and 6-layer through-hole
Suitable Products
RZ/G
  • Was this article helpful?