Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is it possible to turn the power supply of Cortex-A7 cores of the RZ/G1E off?

Latest Updated:05/09/2016

Question:

Of the two built-in Cortex-A7 cores of the RZ/G1E, is it possible to turn the power supply of one core off and operate while supplying power only to the other core?

Answer:

It is not possible to turn off the Cortex-A7 power supply. 
Suitable Products
RZ/G1E
  • Was this article helpful?