Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can each capacity of cache and RAM built in the SH7727 be shared?

Latest Updated:03/25/2009

Question:

Can each capacity of cache(16KB) and RAM(16KB) built in the SH7727 be shared?

Answer:

Since the cache and built-in RAM of the SH7727 are independent modules, they can not share their capacity mutually.
Suitable Products
SH7727