Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Do I have to set registers such as the PFC to enable the weak keeper?

Latest Updated:12/22/2010

Question:

As the MCU includes unused pins (pins with weak keeper), I would like to enable the weak keeper function to reduce external pull-up or pull-down resistors.

Do I have to set registers such as the Pin Function Controller (PFC) to enable the weak keeper?

Answer:

Register setting is not required. Weak keeper function of pins with weak keeper is always enabled, regardless of register setting.
Suitable Products
SH7265
SH7263
SH7206
SH7205
SH7203