Does the SDRAM possible to be used as display memory for LCD?
Latest Updated:03/24/2009
Question:
Is only the synchronous DRAM (SDRAM) possible to be used as display memory for LCD?
Answer:
When using LCD controller, the display memory supports only the
synchronous DRAM (SDRAM) connected to the area 3.
synchronous DRAM (SDRAM) connected to the area 3.
Suitable Products
SH7727 |
SH7720 |