Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

From which cycle is data outputted in the extension of CS assert term?

Latest Updated:03/23/2009

Question:

Regarding the operation in the extension of CS assert term, when CS assert additional extension is carried out in the setup of address /data multiplexer I/O space, which cycle is the data outputed from?

Answer:

SH7065=>The writing data is output from the Th cycle.

Except the above => The writing data is output from the T1 cycle.

Suitable Products
SH7065