Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How is the TxD pin after serial transmission in Synchronous mode?

Latest Updated:03/25/2009

Question:

How is the state of the TxD pin after serial transmission in Synchronous mode?

Answer:

The TxD pin holds the data of the final output after the serial communication.
Suitable Products
SH7144 Series
SH7060 Series
SH7065
SH7050 Series
SH7058
SH7055
SH7047 Series
SH7046 Series
SH7040 Series
SH7030 Series
SH7020 Series
SH7010 Series
SH7018
SH7011