Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How should Pin 99 be handled for the SH7045 Flash and Mask Rom versions ?

Latest Updated:03/18/2009

Question:

How should Pin 99 be handled for the SH7045 Flash and Mask Rom versions ?

Answer:

For SH7045F (Flash) Pin 99 is the FWP terminal. For the Mask-Rom version SH7045, Pin 99 must be set to Vcc. This pin is actually an input terminal and it must be set directly to Vcc or via a pull-up resistor.
Suitable Products
SH7144 Series
SH7047 Series
SH7046 Series
SH7040 Series