Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How to select pin through AUDATA3 to 0, AUDCK, and AUDSYNC? with others?

Latest Updated:03/23/2009

Question:

How should I select these pin functions though the pins of AUDATA3 to 0, AUDCK, and AUDSYNC# are shared with other functions? I cannot set for the pin function controller.

Answer:

The pins of AUDATA3 to 0, AUDCK, and AUDSYNC # are effective for only the time debugs equipment such as E10A-USB is used (When you input in the low level to ASEMD # pins)

Because it is a pin for debugging, setting with program is not necessary.

Suitable Products
SH7206
SH7206