Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is it possible to rewrite the TCNT while MTU is being counted?

Latest Updated:03/26/2009

Question:

Is it possible to rewrite the TCNT (timer counter) while MTU (multi function timer pulse unit) is being counted?

Answer:

Rewrite the timer counter of MTU after timer counter is stopped.
Suitable Products
SH7144, SH7145
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017
SH7011