Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is operation in True IDE mode possible in the PCMCIA of SH7727/SH7720 ?

Latest Updated:03/23/2009

Question:

In the PCMCIA interface of SH7727/SH7720, is the operation in the True IDE mode possible?

Answer:

The PC card controller (PCC) in addition to the PCMCIA interface supported by bus state controller (BSC) is also built into SH7727/SH7720.

The bus state controller's PCMCIA interface and PC card controller support "IC memory card and I/O card interface" provided by the JEIDA specification Ver4.2 (PCMCIA2.1).

Neither supports the TrueIDE mode.

Suitable Products
SH7727
SH7720