SH7040 wait pin input: What if the setup and hold times are not met ?
Latest Updated:03/18/2009
Question:
SH7040 wait pin input. What happens if the setup and hold times are not met ?
Answer:
In general, if the WAIT input changes between the setup and hold time, it cannot be guarranteed that a WAIT cycle will be inserted by the BSC. There is no danger of latchup in this case however.
Suitable Products
SH7144 Series |
SH7047 Series |
SH7046 Series |
SH7040 Series |