Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

To which is PCMCIA mapped, Area5 or Area6?

Latest Updated:03/23/2009

Question:

To which is PCMCIA mapped, Area5 or Area6?

Answer:

Any location of area5 and area6 can be specified.

When using MMU, PCMCIA interface type can be set in page units.

At this time, the regions are accessed by the values of PTEA set in page units.

When not using MMU, the regions are always accessed by the values of SA 2-0 of PTEA.

(PCMCIA interface type cannot be set in page units.)

Suitable Products
SH7751R
SH7751
SH7750S
SH7750R