Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the maximum capacity of the SDRAM connectable to SH-3/SH3-DSP?

Latest Updated:03/23/2009

Question:

What is the maximum capacity of the SDRAM connectable to SH-3/SH3-DSP?

Answer:

Area 2 and Area 3 of SH-3/SH3-DSP are connectable to the SDRAM and each area has max. 64M bytes of memory space. Max. 128M bytes of the SDRAM can be connected by specifying the SDRAM as the memory type to connect to Area 2 and Area 3.
Suitable Products
SH7729R
SH7727
SH7709S
SH7706
SH7705